1/21/2025 1:39 PM | |
Joined: 8/3/2009 Last visit: 9/1/2025 Posts: 16284 Rating:
|
Hello this is a quite normal behaviour if you do not have stored already some parametersets. in the drop down list you will only see the already stored parametersets. So you have to create one and set the values you want to store and then save the settings. Or you can upload the values from the PLc then use the button for loading the values from PLC. Than also you have to store the values in a prameterset. If you have a few parametersets you can select one and then download to PLC. If you need general help at this topic then check the manual or also this FAQ: https://support.industry.siemens.com/cs/de/en/view/109821886 Bye Murof |
If this Information really helps, you could use the Rate function |
|
1/22/2025 12:44 AM | |
Joined: 4/17/2022 Last visit: 3/7/2025 Posts: 22 Rating:
|
Hello I can make sure,we created and stored,it's in production missing and I will check as follow the FAQ. |
1/23/2025 6:25 AM | |
Joined: 4/17/2022 Last visit: 3/7/2025 Posts: 22 Rating:
|
Hi I have a another question,Is the number of parameter set type generated by automatic? What is it's function and What does it do ? Please see the attached. |
Follow us on