1/9/2025 3:06 PM | |
Joined: 7/11/2024 Last visit: 8/4/2025 Posts: 200 Rating:
|
Hi Mr_Prof I think that the easiest solution is to create a screen with an "Alarm view" object and, in case the connection fails, you will be able to see an alarm as explained here: Procedure if there is no connection Hope it helps! |
Last edited by: JimHalpert at: 01/09/2025 15:07:05If this post has been useful, don't forget to rate it!😊 |
|
1/9/2025 3:45 PM | |
Joined: 2/26/2024 Last visit: 8/6/2025 Posts: 130 Rating:
|
The requirement is that if the HMI loses connection. |
Last edited by: Mr_Prof at: 06/15/2025 17:41:40 |
|
1/10/2025 2:09 PM | |
Joined: 4/26/2012 Last visit: 9/4/2025 Posts: 1645 Rating:
|
Hello, I saw that there is this option in V20, I haven't been able to test it yet, if you do, give us feedback here. Look in the System tags for the @ and locate the connection and "_PLC_OpState" value 8 is run PLC The status is for lost communication and PLC in stop. Good luck.
AttachmentVideo_1736521452.wmv (111 Downloads) |
Last edited by: rdoliveira at: 01/10/2025 14:09:35edit Last edited by: rdoliveira at: 01/10/2025 17:13:36edit Last edited by: rdoliveira at: 01/10/2025 18:06:05video Last edited by: rdoliveira at: 01/10/2025 18:20:25edit "Always make a backup before performing any tests |
|
Follow us on