2/3/2025 10:02 AM | |
Joined: 9/23/2005 Last visit: 9/3/2025 Posts: 4416 Rating:
|
Hi As from TIA V20, it is possible to automatically save the custom changes to the alarm control, trend control and f(x) trend control in the user profile, e.g. changes to the position and column width. The changes are available to the user again after the screen is changed or re-loaded. TIP:
Sample project (archived from TIA Portal as .zap20 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! PC-System_1 => persistence activated PC-System_2 => persistence deactivated AttachmentPersistence_20250103_0939.zip (111 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on