8/24/2022 12:41 PM | |
Joined: 5/6/2010 Last visit: 9/8/2025 Posts: 2031 Rating:
|
Hello, which LED is flashing or which is on? It could be that all modules are passivated. If not then do you have a failure at all channels of your input moduel with the result that the inputs are passivated. If you switch off/on then you reset the passivation. Otherwise can you use the function ACK_REQ to reintegrate the modules to the system Please look at the manual SIMATIC Industrial Software SIMATIC Safety - Configuring and Programming at chapter 6.5 regards |
This contribution was helpful to
1 thankful Users |
8/24/2022 1:49 PM | |
Joined: 8/11/2014 Last visit: 8/29/2025 Posts: 4 Rating:
|
clear, Thank you all |
Follow us on