3/26/2025 9:33 AM | |
Joined: 8/8/2019 Last visit: 8/28/2025 Posts: 9 Rating:
|
Createscreenshot function will save it as a PNG (not a pdf). It may be good enough for you? |
3/26/2025 11:23 AM | |
Joined: 1/21/2013 Last visit: 9/8/2025 Posts: 4091 Rating:
|
Hi John, The StoragePath parameter of the CreateScreenshot method must be a complete path name. For a USB stick on the X61 interface this would be /media/simatic/X61/. A possible parameter value would therefore be /media/simatic/X61/screenshot.jpg. To convert the image file into a PDF file, you can use the PDF printer. However, since there is no system print function yet, you would have to create your own lp command call within a method call of the StartProgram. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on