8/31/2023 7:27 AM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16290 Rating:
|
Hello atul.cvs here are some general information, perhaps it helps: https://support.industry.siemens.com/cs/ww/en/view/47756141 bye Murof |
If this Information really helps, you could use the Rate function |
|
8/31/2023 8:19 AM | |
Joined: 3/30/2020 Last visit: 9/2/2025 Posts: 5416 Rating:
|
The problem statement does not have enough information to give a focussed guidance. My first instinct is to ask you about the drive configuration. Specifically if the drive is set to use the communication setpoint. But instead of playing the 20-questions game have a look at the following documents.
The documentation that goes with the first link is very complete. PLC and drive sides are documented and also notes on the connections. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
Follow us on