4/7/2025 4:26 PM | |
Joined: 7/3/2023 Last visit: 8/23/2025 Posts: 3 Rating:
|
Good morning/afternoon/evening/Night, Can you please explain a bit more on this topic, please? I'm a beginner in this field, and I have a little problem similar to this. I've prepared those separate classes of those PLCs, and I'm stuck with what to do next. I've thought of going with the pop-up method, but if the number of PLCs increased, it would be too much for me to write that code, and I've done similar pop-up code for opening 9 no. PLC values, and if he selected one, then only PLC 1 values are going to show due to the pop-up screen, and I'm using "Show Property Value with Visible 0 and 1," depending upon what I need to show, but that's a lengthy process... Please help me with this one. I'm no coder; I'm just learning ladder logic now, and I'm also having the same problem with trends too... if client selected plc 1 and he needs to see, print or send an email of that particular plc within a period of time, I'm doing this in Unified RT PC V18. Thanks a lot ------------------------------------------------------------------------------------------ |
Last edited by: levi_marshall099 at: 04/07/2025 16:28:04Last edited by: levi_marshall099 at: 04/07/2025 16:33:47Last edited by: levi_marshall099 at: 04/07/2025 16:34:43Last edited by: Moderator_Lan at: 04/08/2025 07:29:57New subject after splitting |
|
4/9/2025 12:12 PM | |
Joined: 8/3/2009 Last visit: 9/4/2025 Posts: 16343 Rating:
|
Hello levi_marshall099 A way of sending emails in connection with alarms could be to use Alarm Control Center. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on