2/6/2025 1:39 PM | |
Joined: 1/11/2023 Last visit: 7/29/2025 Posts: 2 Rating:
|
I took this a step further and realized that onMouseDown and onMouseUp should have worked, I just used hmi-event:mousedown instead of hmi-event:down. More importantly I figured out how to get any paramter back to runtime through the interface. Let's say we have this parameter
The next line will influence "example" inside the svghmi but it won't affect the value in runtime
However we can write it straight to the Properties
and then we can read out the value using
Few thing to mention:
Attached a slightly modified version of my previous upload that utilizes MouseDown also. Just drop in, add 2 IO-fields with the process value scripts:
Attachmentcoordinatesniffer2.zip (175 Downloads) |
Last edited by: Pitykee at: 02/06/2025 13:40:30 |
|
This contribution was helpful to
1 thankful Users |
Follow us on