4/23/2025 1:56 PM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16343 Rating:
|
Hello Wayse2 first of all do I understand correcly you have installed Unified V19 on your Win10 and then you updated to Win11 on this system? I would not recommend doing this. you can never say what happens to all your installed SW... If you want to reset all your certificates you can do the following. - delete all server certs in IIS - delete the CA in the WInCC Unified Cert Manager - restart PC - create a new CA , device and Webserver Certifiacte in Unified Cert Manager (https://support.industry.siemens.com/cs/de/en/view/109806850) - Install all Certs in the Cert manager and do also export the CA (in V19/V20) and install it to the list of trusted cert stores - restart PC - Run the Unified Configuration dialog and select the new webserver certificate - do a restart or a logon/logoff I often used this if a system was working with corrupted configuration of certificates (So far it works every time in different Versions) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on