5/2/2025 7:50 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi TheZoonder, I would not recommend copying the project from an existing runtime instance to another machine. I am afraid this would not work because I do not expect loading a runtime to be a simple file transfer operation. So you should add the project from an external storage medium to the runtime. But this may not work for a simulation. However, since you seem to have a problem with the user rights on the computer, you can test by configuring a SIMATIC WinCC Unified RT system. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on