5/1/2025 4:25 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi TommyT15629, Unfortunately, the HMI Template Suite WinCC Unifed is currently only available for public download in V19 and V20. This means that you are probably using the WinCC Comfort/Advanced V17 Template Suite, which is not compatible with WinCC Unified. You can try to get an archived version by creating a support request. Or you think about an update of your engineering system, which will bring more functionality with more performance and stability, especially in the context of WinCC Unified. Kind regards |
5/7/2025 8:40 AM | |
Joined: 8/3/2009 Last visit: 9/1/2025 Posts: 16284 Rating:
|
Hello TommyT15629 Unified and Comfort/Advanced are totaly different systems You can try to convert some project contect with the tool Data2Unified but this will not migrate it 1:1 and you will have a lot of work to adjust the details. You should think also about starting a new layout of your screens with Unified. bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on