5/14/2025 8:59 AM | |
Joined: 8/3/2009 Last visit: 9/3/2025 Posts: 16303 Rating:
|
Hello AutoGen_2251034 If the problem occurs in V20 with all projects (also with a new testproject), then do you have installed allready the latest Update in TIa Portal ? I did a quick test with my TIA v20 Upd1 with a MTP1000 Unified Basic Panel - create a testproject and download it to the panel -> It took about 2-3 seconds to load to the panel If you have only problems with a special project you can try to delete the temp data: https://support.industry.siemens.com/cs/de/en/view/109778709 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on