2/18/2025 7:24 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi, There will be several approaches depending on the items being used. Assuming a polygon is used, you can use the "BorderColor" property. Alternatively, you can simply write a tag and use that tag within the border color dynamization. Kind regards |
2/19/2025 2:45 AM | |
Joined: 11/28/2024 Last visit: 6/15/2025 Posts: 43 Rating:
|
Hi, Using three polygons, but on selection from the dropdown values the desired border should be highlighted that is tags used for the border will be from the digital outputs and the drop down tags assigned are the input tags. But this approach is not working. Any solution? |
5/14/2025 11:36 AM | |
Joined: 9/23/2005 Last visit: 8/27/2025 Posts: 4416 Rating:
|
Hi 1 - Use a graphic list, this solution needs a graphic / tag value for each status combination. Exemple in WinCC Unified – Simple Sample - Text List / Graphic List 2 - Use a combination of several independent objects and acts (cynamize) his properties. This will still needs tags to relate the status to the proprieties. |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on