5/28/2025 5:46 AM | |
Joined: 10/17/2024 Last visit: 9/2/2025 Posts: 5 Rating:
|
I am currently working on the Master Data User Forms using WinCC 8.0. I would like to implement adelete optionthat allows users (e.g., an admin) toselect existing data and delete itdirectly from the UI. For example, if the admin has previously added a grade type, there should be a way to select that entry and remove it as needed. I've attached a screenshot for your reference. Could anyone please guide me on how to achieve this functionality in WinCC 8.0? Thanks in advance for your support AttachmentwinCCScreenFDS.zip (100 Downloads) |
6/4/2025 11:15 AM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16343 Rating:
|
Hello FarheenQ I know this example is for TIA Portal and an Advanced RT. but the way of deleting data with the ODBC connection is basically shown. So you cannot use this 1:1 but it will have all the needed steps https://support.industry.siemens.com/cs/de/en/view/61883659 perhaps it helps Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on