10/31/2023 12:44 PM | |
Joined: 11/2/2008 Last visit: 8/30/2025 Posts: 95 Rating:
|
Hello Everybody, I am using V90 servo with S7-1200 CPU on TIA V16 This happening with us second time. When we changed following settings in the axis configuration of the TO 1. Selecting "Invert Encoder Direction" 2. Changing the Encoder type to "Linear Absolute" We observed that after changing these parameters at different instances, And Enabling the drive in Commissioning mode of TO Motor started rotating at Full speed without giving any command. We restored this after resetting drive to factory default and also resetting TO object. Please suggest solution to this, as at first instance our mechanical system also got damaged. Thanks and Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/02/2023 07:11:00New subject after splitting |
|
Follow us on