9/3/2025 11:18 AM | |
Joined: 8/3/2009 Last visit: 9/3/2025 Posts: 16322 Rating:
|
Hello In WinCC Unified there is also a ChangeConnection systemfunction, so the soluino for the common Comfort Panels should also work with a Unified system: https://support.industry.siemens.com/cs/ww/en/view/96837136 Its not 100% the same because you do not have direct tag trigger like in WInCC Comfort/Advanced but with screenlocal triggers or also scheduled task you should be able to adapt the solution in Unified bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on