6/24/2010 11:10 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Check suggestion in both threads: 1. E Display on PMU of inverter 2. E Display on PMU of inverter - After one day the same old problem is there Check connection cable with PC. Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
6/24/2010 11:16 AM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Hi, Regarding your problem, few steps to be check 1) Are you connected with drive with drive PC Cable? If yes then try removing this cable 2) If you have given 24V only, try giving DC voltage to the drive because this problem may come if your 24 V supply is being loaded 3) Try Swapping PSU, IVI boards if possible Check following forums for further Help /tf/WW/en/Posts/30290#top Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
1 thankful Users |
6/24/2010 11:19 AM | |
Posts: 109 Rating:
|
Thanks for quick reply UMENCHO/VITHANI |
This contribution was helpful to
1 thankful Users |
6/25/2010 9:41 AM | |
Posts: 109 Rating:
|
I replaced PSU card with Spare one and Problem get solved... Thanks for the Help Regards, |
This contribution was helpful to
3 thankful Users |
Follow us on