6/25/2010 10:56 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi JamesB, The Siemens Part number (also known as MLFB) contains 0's (zero's) and not o's (the letter o). If you enter any o's, you will not get the correct responses from the Mall etc. A little history . . . . . . In the early days, there was: CU1 (FC) - Frequency Control CU2 (VC) - Vector Control CU3 (SC) - Servo Control The number i.e. CU1, CU2 relates to the drive 6se70xx-xxx1x or 6se70xx-xxx2x. Basically, the FC and VC versions have become the modern CUVC, and the SC became the CUMC version. You are correct, there is only one manual for the modern VC drives i.e. 6se70xx-xxx6x. You can download the latest version of the VC Compendium here I have attached the early FC manuals, and due to the size restrictions, I will post the Early VC manuals next post. Hope this helps, Graeme AttachmentEarly_FC_Manuals.zip (448 Downloads) |
This contribution was helpful to
4 thankful Users |
6/25/2010 10:58 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, Early VC Manuals
AttachmentEarly_VC_Manuals.zip (429 Downloads) |
6/28/2010 1:11 PM | |
Posts: 14 Rating:
|
Thanks so much. That is extremely helpful. |
Follow us on