12/7/2009 10:25 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User saraowrote: hello sir? i need help for all of you guyz, i have encountered a problem about the downloading parameters from cuvc 3.3 nor 3.4, i used drivemonitor 5.2.2 and i upload succesfully the parameters from old cuvc sw.3.2. now i downloaded it to a new firmware version 3.3,but i cant downloaded succesfully i had a message recived ERROR: Download ValueFailure PNR 71[0] [F-No.:104] ERROR: Download ValueFailure PNR 102[255] [F-No.:104] ERROR: Download ValueFailure PNR 128[255] [F-No.:104] ERROR: Download ValueFailure PNR 274[255] [F-No.:104] ERROR: Download ValueFailure PNR 319[255] [F-No.:104] ERROR: Download ValueFailure PNR 396[255] [F-No.:104] ERROR: Download ValueFailure PNR 525[255] [F-No.:104] but before me start download the parameters drive monitor ask me about the conversion of a firmware version and i click ok but the same error after finish from downloading. pls sir can you give me a reply about my problem? |
12/8/2009 2:43 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
All the mentioned parameters belong to drive- and motor-settings. |
12/9/2009 7:34 AM | |
Joined: 9/20/2006 Last visit: 8/1/2025 Posts: 307 Rating:
|
have you manually programmed the value of P70 befor the downloading process. Where are you from ? Diwa. |
7/5/2010 11:55 AM | |
Posts: 33 Rating:
|
had exactly z same two minutes ago and am working on it .. I believe God "ALLAH" will help me and i'll come bk to u soon |
Follow us on