11/24/2010 11:40 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Try my example. Best regards, Hristo Mihalev AttachmentAbb1.zip (1222 Downloads) |
11/24/2010 1:38 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi Tagolover, or can i directly trasfer the word value to the input/ ouput address of the drive will it work Yes, you can used the same way used for the Siemens Drive, just need to change the Setting in related to the Drive side & Value coming from the Drive Status as Comapre to SFC14 & 15 it is easy.. try to do it with the VAT Table, so you will get the fell of it. or MICROMASTER 4 & SINAMICS G Function block (FC14) to control an MM4 via Profibus-DP |
Last edited by: Ammy at: 11/24/2010 1:39 PMAmmy |
|
Follow us on