2/8/2011 10:51 AM | |
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
Dear Sir We have one project of Building Management System (BMS). In this project we have different type of devices which have different communication protocol Such as RS485,CAN,Modbus,Profibus,Ethernet. I want to the convert all protocol with profibus of all devices for Siemens S7-300 or 400 PLC. I have following Devices in this project Technical Specification is under. What will you Suggest the Siemens Hardware & Software for following Application. 1= 08 Control Module with RS 485 Modbus protocol (Make Deap Sea UK) 2= 38 Power Analyzer with Profibus Protocol (Make Janitza Germany) 3= 07 Power Factor Controller with Profibus Protocol (Make Janitza Germany) 4= 05 MKIV Elektronikon Control Module with CAN Protocol (Make Atlas Capco) 5= 10 Temperature,RH,Flow & Pressure Transmitter will be access with Simatic PLC Station Comprising Profibus Protocol (Make Siemens) 6= 02 MCC (Motor Control Center) Status Monitoring & ON/OFF Controlled will be access with Simatic PLC Station Or Distributed I/O with Profibus Network [schnippschnapp] other questions are splitted to SCADA: Basic questions. Thanking you & assuring you of our fullest cooperation & prompt attention at all times. Regarded Muhammad Sarfraz |
Last edited by: O_Moderator at: 2/8/2011 11:21 AMnew subject after splitting MS |
|
2/8/2011 1:20 PM | |
Joined: 9/23/2005 Last visit: 9/4/2025 Posts: 5112 Rating:
|
Have a look there. |
Regards, |
|
2/12/2011 7:55 AM | |
Joined: 10/7/2005 Last visit: 9/4/2025 Posts: 3049 Rating:
|
Hello Sarfraz Bhatti I can't speak for the ADFweb gear (haven't used it yet), but in case you won't find what you are looking there or need an alternative, Isuggest to have a look at www.hms.se and use an ANYBUS Gateway (I only had good experience with their gear thus far). I hope this helps and good luck |
Cheers |
|
Follow us on