6/1/2011 7:16 AM | |
Joined: 2/20/2007 Last visit: 11/19/2024 Posts: 122 Rating:
|
Hello, Did you mean to say, you want to configure digital input as a Hard wire E-stop. If yes, then which digital input you want to configure. If its Digital Input 0:then parameterize P701=2 or 3 (OFF2 or OFF3) If its Digital Input 1:then parameterize P702=2 or 3 (OFF2 or OFF3) and so on. Please refer page no 64 in the attached manual Hope this helps. Regards, Ahmed AttachmentG120_Parameter Manual.pdf (632 Downloads) |
Follow us on