12/15/2006 8:22 AM | |
Posts: 2348 Rating:
|
Could you please be more specific? Uploading zipped project may be helpfull. |
12/15/2006 9:27 AM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi, you should know that the data records are storaged on the panel or on the PC. If you want to transfer to the plc you need the system function "SetDataRecordTagsToPLC" or "SetDataRecordToPLC". You can get more information about recipes in this link: ![]() http://support.automation.siemens.com/WW/view/de/23901413 I think that you find a solution of your problem in this description. ![]() Bye |
12/15/2006 10:11 AM | |
Joined: 12/14/2006 Last visit: 6/16/2025 Posts: 7 Rating:
|
The project is here! On the page1 i have write the informations. On the "change value" of the tags "Control_Read" and "Control_Save" the function "LoadDataSet" and "SaveDataSet" are executed. I'm using this for reading the parameters of profibus slaves. The number and the index of the parameter to read is stored in the recipe. PLC reading the value of the parameter. I would want to save the value in the recipe and export it on CSV file |
12/19/2006 8:07 AM | |
Posts: 2348 Rating:
|
Try to mark Control_Read and Control_Write as "read continuosly" tags - then you dont need those switches? |
Follow us on