9/13/2011 2:25 PM | |
Posts: 65 Rating:
|
Hi, This is raghu. Am having problem with S7200 and MM440 Drive through USS Communication. Frequently drive showing F0060. It means communication problem. And most of the time in HMI am getting ### where which i can monitor drive speed. What could be the reason behind that. Recently i got USS library V2.3 but i hiven't used that lib. Still Machine is running in the Old uss libraries only. How to use the new version library. And what could be reason for frequent communication failure. Please Solve my problem. Thanks in advance, Regards, Raghu Splitted from USS Communication using USS Library V2.3. |
Last edited by: O_Moderator at: 9/14/2011 9:31 AMnew subject after splitting |
|
9/18/2011 5:24 AM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
I think there is problem in Internal 24V supply Please have a look at following Discussion /tf/WW/en/Posts/9430 http://support.automation.siemens.com/WW/view/en/8822493 /tf/WW/en/Posts/49308 https://support.automation.siemens.com/WW/llisapi.dll?query=F0060&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8&cssearchengine=NEW Regards, Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on