10/21/2011 9:28 AM | |
Posts: 739 Rating:
|
Hello, it is not enough to set up the controll parameter for USS, you have to configure the USS-protocol (p2009 – p2013). Pls. follow the instructions of the MM440-handbook (chapter 3.7). http://support.automation.siemens.com/WW/view/en/24294529 Further information pls find in the FAQ (ignor the mentioned MICROMASTER!): How do I read and write parameters to the MM420 using USS? http://support.automation.siemens.com/WW/view/en/5280592 What information is available about using USS Protocol with the MM420? http://support.automation.siemens.com/WW/view/en/5734889 Recommendations for reliable RS485 communication between S7-200 and MICROMASTER 4 / SINAMICS G110 / SINAMICS G120 http://support.automation.siemens.com/WW/view/en/30559069 |
Follow us on