4/26/2012 4:14 PM | |
Posts: 7 Rating:
|
Hello everybody! AttachmentSchéma des connexions35.zip (387 Downloads) |
4/27/2012 9:14 AM | |
Posts: 7 Rating:
|
hello marcjan thanks for your answer! your tactics doesn't work... have you other tricks? this situation annoys me |
4/27/2012 10:39 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, I noticed that too, Seems you have made constructions in Lad that can't be converted to FBD without these errors. Since the program is transfered to the Logo in FBD, you have a problem there Don't know if the program will still work if you solve the errors with open connectors, the oba6 Logo has them (16) you can use and blocks to combine 4 open outputs. Test it in simulation, you know what the program should do. If not working i see no other option than build the program again, do yourself a pleasure and use FBD then ! No ladder for me and many others here. Perhaps some Logo Cracks now a solution, let's see. Regards Marcjan AttachmentSchéma des connexions35-without error.zip (384 Downloads) |
Last edited by: Marcjan at: 4/27/2012 10:42 AMProblem solved? |
|
5/8/2012 9:57 AM | |
Posts: 153 Rating:
|
Hi,Steph68..and what version of the program lofo!soft? You can write. |
Follow us on