10/23/2012 8:47 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Is the problem you miss or get double counts? Is that in simulation or in real PLC. Showing us what you created is a good idea to solve your problem. Attached file is what you want to do? Regards, Marcjan Attachmentcount_forum.zip (367 Downloads) |
Problem solved? |
|
10/23/2012 12:30 PM | |
Joined: 12/27/2006 Last visit: 8/26/2025 Posts: 1200 Rating:
|
Something like my programm?Attachmentteller2.zip (364 Downloads) |
10/23/2012 6:51 PM | |
Posts: 4 Rating:
|
Well, Marcjan is close but i would like to do it with only 3 timers. That way i only have to chance the first one to for example 5, the second timer will stay the same and the third will count the 1 to 4 pulse. this is what i first tried to do, easy, simple, logic, but doesnt work You will see that the first counter has a slight delay with his output making that he gets the pulse before block B04 can say it may not count.. On the otherhand.. What Toeternitoe showed in his program is a thing i've never seen before, so thanks for the example... And third, is it me or are u boyh dutch? As a beginning (trying) programmer it would be nice to know what u guys use it for and in what branche? As for now we will say its an tie between u guys for who gets it first game on... Attachmentcounter try.zip (291 Downloads) |
10/24/2012 8:48 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, O.k. i changed your program a bit, hope this is what you need. And yes i'm Dutch, it's not a secret Regards, Marcjan Attachmentcounter_try_1.zip (283 Downloads) |
Problem solved? |
|
10/24/2012 7:03 PM | |
Posts: 4 Rating:
|
Thanks Marcjan, your program worked, but when i changed te 3x pulses to another number or to 1, it doesnt anymore. Its because a have to count the wheels of the chain inbetween the ones that are greased. to we need to change the number as aesy as possible. (just in 1 counter) I also changed my own program and it was easier then i thought. thanks very mutch for the help but i'll keep the thropy.... Try it and look if you find it good or can make it even more better greetz Attachmentcounter finished.zip (333 Downloads) |
Follow us on