2/1/2013 2:14 PM | |
Joined: 10/11/2006 Last visit: 9/5/2025 Posts: 6038 Rating:
|
Dear Mr. / Ms Mnada, P700 serial bus adress Indices: i001 = SCom1: bus address of the ser. interface 1(CU) , on the PMU mostly used for the drive monitor communication. Mostly 0 due toconverter - DRIVEMONITOR coupling. (Depending on the pin RS485 or RS232). i002 = SCom2: bus address of the ser. interface 2 (CU), on -X101 pin 10, 11, 12 (RS485) i003 = SCB: bus address of the SCB, if P696 = 1, 2 |
With best regards, |
|
Follow us on