6/9/2007 9:32 PM | |
Posts: 57 Rating:
|
I have enclosed screenshots of a trendview and the corresponding variable values in a csv-file. The problems concerns the trendview in the time period of 07/06/2007 13:45. In screenshots 2 and 3 I have put the ruler at that time value, but the screenshots are from scrolling in the trendview. In screenshot 3 the correct value is represented, in screenshot 2 a corrupt value, this can be checked in the csv-file. The trendview is based on the logfile, logging is triggered on change of value. I tried dotts for value representation in spite of lines, but the same corrupt values were represented. In the time period of the corrupt values, the runtime was not stopped (running on a pc, WCC Flex runtime SP1 HF7, bought in march 2007). It seems an interpolation problem in the trendview. Probably the corrupt values are always behind the last logged value in the trendview screen (newest values from the right). Is there any way to avoid this problem, or is it a system problem? Thanks. AttachmentTrendview.zip (198 Downloads) |
Follow us on