5/17/2013 10:00 AM | |
Joined: 10/11/2006 Last visit: 9/5/2025 Posts: 6038 Rating:
|
Hello, For the communication i would suggest to use telegram 352. It contains all the informations you want. (See Attachment). For the communication you can use some of the application example which can be found here: http://support.automation.siemens.com/WW/view/en/34677186/ If you don´t find a suitable application you can maybe use an example regarding S7-300 and G120. |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on