5/26/2013 3:11 PM | |
Posts: 7 Rating:
|
This down counter is only for 0BA6 + It is not possible with lower versions :( I have 0BA4 and I am trying to downcount & write on displays downcounting on unit but did not find any solution ... |
Last edited by: O_Moderator at: 5/27/2013 1:49 PMnew subject after splitting from /tf/WW/en/Posts/42578#top |
|
5/27/2013 7:58 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, The 0BA4 doesn't allow a startvalue in the counterblock, you can create a startvalue yourself. Please have a look at attached program. Regards, Marcjan Attachmentdown counter 0BA4.zip (326 Downloads) |
Problem solved? |
|
5/31/2013 8:56 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi all, i have some comments to the given solution and i have build a modified version V2 with: - cleared unneeded blocks The result is file "\DEMO_down counter_V2 0BA4.lsc" at the attachment. Attachmentdown counter_V2 0BA4.zip (286 Downloads) |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to
1 thankful Users |
6/7/2013 9:40 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi dinac, yes the LOGO!-series 0BA6 and 0BA7 has Blocks counter with start value to set be every reset the block. But ther is no possibility the set a step with - ol the time the counter counts only the impulses at the input pin. Only with a circuit you can built n impulses for the counter by one puls as input signal. a) use a block "Edge triggered wiping relay"to build 1 to 9 pulses with smalest values of Th and TL b) faster, but needed more blocks, you use the technique i showed you before with the preset counter to build impulses witch need only two LOGO!-cycles (and not 0,02 s) Please remember: a) and b) have restrictions to the speed of the input impulses! Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
Follow us on