7/5/2013 1:17 PM | |
Joined: 2/6/2009 Last visit: 9/1/2025 Posts: 940 Rating:
|
Hi, Can anyone please help me to convert the below S7 block into the S5 logic. The below blocks was developed by me only, bit it is very difficult for me to convert the same into S5 logic since it contains indirect addressing. Matter is very urgent, please help!
AttachmentFC1.zip (351 Downloads) |
_______________________________________________________________ |
|
7/5/2013 2:12 PM | |
Joined: 7/15/2008 Last visit: 3/13/2025 Posts: 382 Rating:
|
What S5 Processor are you intending to use this for |
7/5/2013 2:45 PM | |
Joined: 2/6/2009 Last visit: 9/1/2025 Posts: 940 Rating:
|
S5 115U |
_______________________________________________________________ |
|
7/16/2013 6:07 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hi Saravana kumar These Attachments are Extracts from S5-115U Manual giving detailed explainations and sample programs for : a) "DO" Instruction for Indirect addressing b) LIR/TIR/LDI/TDI/TNB - Instructions for DIrect memory access Hope these help you in formulating your program Cheers Navnag AttachmentS5_Operations.pdf (579 Downloads) |
There is no such thing as the last bug in a program |
|
Follow us on