2/15/2012 7:26 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Looks like you have installed the wrong driver, 64 bit one, did you install these manualy or automatic when asked? What interface cable you have there? You can try download driver here https://www.automation.siemens.com/mcms/programmable-logic-controller/en/logic-module-logo/application-examples/Pages/Default.aspx Regards, Marcjan |
Last edited by: Marcjan at: 2/15/2012 7:35 AMProblem solved? |
|
7/17/2013 11:34 AM | |
Posts: 10 Rating:
|
I solved a similar problem by updating Logo V7.0 to Logo V7.1 |
7/17/2013 3:56 PM | |
Posts: 378 Rating:
|
In the windows device manager I can see the com port listed and is OK. Any help is greatly appreciated. Yours Sincerely Karel Hello Karlito, The problem is version mismatch between rxtxSerial.dll and your OS, have a look at this link and you can download and replace the rxtxSerial.dll file that can match your OS. Download: Hope helps, |
This contribution was helpful to
2 thankful Users |
Follow us on