7/24/2013 12:54 AM | |
Posts: 3 Rating:
|
Dear all, Sorry I'm new with this sinamics. According the manual Booksize Equipment Manual in Section 2.8, each wiring diagram Line Contactor is optional. But I would use it. Then I did the following connection: (page 42 figure 1-10) https://www.automation.siemens.com/doconweb/pdf/SINUMERIK_SINAMICS_04_2010_E/FH1.pdf?HTTPS=REDIR&p=1 But the DO 8 (X122.7) is never in 1 so the contactor isn't actived. After reading this document: https://www.automation.siemens.com/doconweb/pdf/SINAMICS_1109_E/LH1.pdf?HTTPS=REDIR&p=1 I see there is the function p0864 before the sequence 3 where the Line contactor is closed and must be in 1. I don´t understand where I must use this Alimentation service in the logic or this connection I can' t see in green or in 1 if I use with r863 bit 0 I attach my proyect. Than you very much AttachmentSiemens_s120_V01.zip (137 Downloads) |
Follow us on