9/9/2013 6:48 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello steffo You need to do the following : a) Provide a small reverse speed setpoint to the unwinder c) Limit Torque in both directions ( Motoring / regeneration ) for Unwinder The Unwider tries to run reverse, however the Winder / other equipment will force it to run in forward direction at the Set Torque limit. This will establish Tension in the Line. Tip : You may need to De-activate Speed Setpoint / Actual value difference monitoring in Unwinder. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on