4/22/2014 11:31 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello Him Check there: Are the binary input command functions RUN right and RUN left the same on the MM4/SINAMICS G120 as on previous MICROMASTER products? |
4/22/2014 11:32 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Have a look at the: Getting Started Guide: MICROMASTER 420/430/440 Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to
2 thankful Users |
5/12/2014 4:56 AM | |
Posts: 28 Rating:
|
Hi change drive parameters P1820 from 0 to 1,then we can operate the motor in reverse direction. Regards aakash
|
This contribution was helpful to
1 thankful Users |
5/13/2014 8:54 AM | |
Joined: 3/15/2011 Last visit: 4/23/2025 Posts: 134 Rating:
|
Hi By changing the Parameters P1820 from 0 to 1 we can reverse the direction, Regards ashutosh |
Follow us on