5/19/2014 8:12 PM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello Bobco Is this what you are looking for : SINAMICS S: Positioning an S120 with S7-300/-400 (STEP7 V5) via PROFIBUS/PROFINET with Safety Integrated (via terminal) Maybe these examples will also help you SINAMICS S120: SINAMICS S120: Controlling Safety Integrated Extended Functions of the SINAMICS S120 via the onboard terminals of the CU310-2 PN SINAMICS S: Speed control of a S120 with S7-300/400 (STEP 7 V5) via PROFINET (PROFINET IRT, isochronous) Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
3 thankful Users |
Follow us on