6/2/2014 8:13 AM |
|
Joined: 9/23/2013 Last visit: 9/11/2025 Posts: 51 Rating:
|
Dear Exper Is it possible to check MM430's-IO card on MM440 drive. Also MM440's IO card on MM430 drive? Thanx |
6/2/2014 2:49 PM | |
Posts: 784 Rating:
|
What is the part no. of each card?
|
6/2/2014 5:38 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
I think its available because i remembered someone from my plant has ordered it. I will confirm later on. More over, link shared by Ste39also says same Although i am still not sure whether same card can be used for both drive. May be some siemens engg can tell us exact - Graeme- its your call.. |
Last edited by: Vithani at: 6/2/2014 5:39 PMonce again stuck in quote I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
1 thankful Users |
6/2/2014 6:29 PM | |
Posts: 89 Rating:
|
Dear Exper Is it possible to check MM430's-IO card on MM440 drive. Also MM440's IO card on MM430 drive? Thanx Hi you can check it as both have same vector IO CARD |
6/2/2014 6:31 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
I think its available because i remembered someone from my plant has ordered it. I will confirm later on. More over, link shared by Ste39also says same Although i am still not sure whether same card can be used for both drive. May be some siemens engg can tell us exact - Graeme- its your call.. Dear Vithani, For I/O board I still doubt that it can be ordered. I found this document -(it is in German) because no English version is available You will found I/O module boards only for Vector Control. I am not sure if that is what you mean or not. Hope this helps.
AttachmentFAQ_MM4_spares_de_V2.pdf (258 Downloads) |
Last edited by: Ayman Elotaify at: 6/2/2014 6:35 PMLast edited by: Ayman Elotaify at: 6/2/2014 6:34 PMAyman Elotaify |
|
Follow us on