6/23/2014 9:44 PM | |
Joined: 3/10/2014 Last visit: 11/28/2023 Posts: 1 Rating:
|
hi dear friends i want using the micromaster 440 by cpu 315u (s5) via profibus .please help me for this job
|
6/23/2014 10:23 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12401 Rating:
|
Hello amir; Please be very precise when you ask a question here, there is no s5315u CPU in the Siemens families of PLCs. If thsis is really a S5 CPU, what family and what Profibus interface are you using? Normally the software used to configure and download teh configuration to a S5 PLC is called Com Profibus, if the interface module is a IM 318C or if you are using a S5-95U's integrated Profibus port.. Do you know if there is an existing Profibus-DP configuration running presently on the S5 PLC, or would this be a new installation? The following manual will give you indications on the steps required to create a Profibus-DP configuration for a S5 Profibus master and how to transform it in the binary file that can be sent to the S5. Also, here are some basic documents and sample programs you can use to strrt understanding the exchage mechanisms used by the MM4 drives using a Profibus-DP interface. Please start by studying them. Various FAQS: MICROMASTER 4 (MM4): What is important when setting up an MM4 with a Profibus module? Operating Instructions: MICROMASTER PROFIBUS Optional Board Various Siemens Applications with sample programs: MM4 and Profibus-DP: http://support.automation.siemens.com/WW/view/en/34677186/136000&cspltfrm=0&cssw=0&csbinh=8 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/23/2014 11:34 PM |
|
Follow us on