9/21/2014 1:39 PM | |
Posts: 2 Rating:
|
Hi, Is it a parameter and do you want to change it? |
9/21/2014 2:02 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, What I presumed is you want to use fixed frequency set points to increase or decrease the speed. If my assumption is correct, you can use/configure DI1 to DI6 with corresponding parameters to set different set points corresponding to fixed frequency. With use of these DI you can vary the speed. For more information, please refer the attached sheet. HTH. AttachmentMM440 Fixed Frequency.pdf (320 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on