10/23/2014 12:35 PM | |
Posts: 211 Rating:
|
Hi all! Will it be fixed soon? I am in a hurry, ordered V4.0 CPU but never get warning that it is NOT compatible with Profibus master module? Thanks! |
10/23/2014 4:32 PM | |
Joined: 7/7/2010 Last visit: 9/4/2025 Posts: 16057 Rating:
|
Contact Support Requestand let them know the firmware revision and part #'s for the PLC and the PB Master Module. There is a firmware revision for the PB master module if I recall correctly that seems to correct lots of problems. You apparently *must* use a Siemens compatible MMC to load firmware to modules like the PB master module. I updated a PB master module recently and asked why the web server firmware update does not work for the modules connected to the PLC. Sadly, they did not tell me, only that the MMC was required. Luckily we keep one on hand for the odd situations like this. |
science guy |
|
Follow us on