10/27/2014 10:21 AM | |
Posts: 3 Rating:
|
I need to configure Master Drive with S7-300 (314-2DP) by profibus, How can I read 1)Act.frequency 2) Act Speed of the motor 3) motor spee/ freuency set point 4) act.power. how can I configure the input and output words in PLC program? Plz help
----------------------------- New subject after splitting from Communication profibus between S7 300 CPU 314 with MM440 inverter. |
Last edited by: Min_Moderator at: 10/27/2014 2:40 PMSplitted |
|
10/28/2014 6:48 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello sulaxmiTechnologies, Have you already seen this: Connection of Masterdrives to Profibus-DP - Siemens Industry ... |
10/28/2014 11:34 AM | |
Posts: 1058 Rating:
|
Maybe this will help: Read/Write parameters from/to an inverter via Profibus DP regards |
Follow us on