3/14/2015 7:09 AM | |
Joined: 2/8/2015 Last visit: 7/10/2024 Posts: 462 Rating:
|
Hi I heared that according to the programs that designed by siemens co, until 2020, the S7-300 and S7-400 PLCs will be omit from the product cycle.And the SIMATIC S7-1500 will be the only producing product by the siemens.( in PLCs ) Is that right? Thanks ---------------------------------------------------------------------------------------------------- Split from s7300 failsafe Closed cause question posted twice. The second thread with the subject S7-1500, S7-300 and S7-400 in 2020 is published within the conference SIMATIC S7 general.
|
Last edited by: Min_Moderator at: 3/16/2015 1:40:12 PMNew subject after splitting and closed |
|
Follow us on