5/31/2016 6:41 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating:
|
I can't download "performance_FC630.zip" and use it.What's my problem? |
5/31/2016 7:33 AM | |
Joined: 10/7/2005 Last visit: 9/17/2025 Posts: 3049 Rating:
|
Hello SM hard to say what your problem is without more information, so my question is: - Do you have a problem downloading it from THIS webpage OR downloading it into your S7 CPU? If the latter is the case, please check what CPU with what Firmware you have and verify that FC630 is released for it as per above link. I hope this helps |
Cheers |
|
5/31/2016 7:35 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, Yes not function, have you tried to Support Request ? |
6/1/2016 8:32 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating:
|
Hello fritz, The CPU which I use is CPU315-2DP with firmware 3.3.11.Now can I use FC630 with this CPU? |
Follow us on