10/13/2016 6:44 AM | |
Joined: 12/18/2014 Last visit: 9/2/2025 Posts: 35914 Rating:
|
There is also a delay with the LOGO!s series 0BA8. How long the time is depends strongly on the network and the cycle time. What time this is, I can not tell you. In the test between 2 LOGO! S with a minimum program, 0.05s were not safe. Times worked, then again not. Only from 0.1s onwards a secure transmission was ensured. As I said, only 2 LOGO!s and a minimum program. AttachmentProject.zip (261 Downloads) |
12/13/2016 3:59 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by jorgengyselinck is split to a separate thread with the subject Multiple logo's, can i use in every logo the maximum netwerk inputs/outputs?. Best regards |
Follow us on