7/25/2017 3:24 PM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating:
|
Hi Helmuth I made your test with IP: xxxx:8080 and there is working with direct RJ45 cable, PC>Logo. ( slower upload but is working) when I try to connect by DNS, the test connection reconize the Logo, but if I try to ask any logo information the popup Connection BM... stay continue active...no connection. When I try to upload new software, it asking me to connect, this work, then again the popup BM...but nothing at all. Web server is full working, with Logo App I can also not connect: Server not found. On Router I have opened the forward port: IP: xxxxxxx:8080 and IP: xxxxxx:8081 and with web server I can connect to the two Logos. Internal port on router I leave the 80, because IF I set also 8080 then nothing is working. Any suggestion how I can resolve to connect by DNS internet? Thanks Attachmentscreen logo TCP.pdf (300 Downloads) |
Follow us on