8/15/2017 9:14 PM | |
Joined: 8/12/2017 Last visit: 7/28/2021 Posts: 3 Rating:
|
Hello Maybe my request sounds stupid. I am desperately looking for BYTE_TO_INT and INT_TO_BYTE functions. Background: I have downloaded an SCL FB which I shall rename with a lower number. When I try to "translate" it (I am not sure about wright english term for german "übersetzen") SCL claims that BYTE_TO_INT was missing. I cannot find it, neither in the downloaded library nor in Step 7 standard functions. The strange thing is that the original FB is running perfectly in PLCSIM and only during SCL "translation" problems are occuring. Even trying to program own BYTE_TO_INT and INT_TO_BYTE FCs with simple MOVE commands does not help as it next complains about wrong data type. (The FCs seam to convert perfectly when tested separately) this is the related SCL line
I am really desperated as in many forums the terms BYTE_TO_INT and INT_TO_BYTE are discussed as if they were standard functions. Where can I find them? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/16/2017 12:27:57 PMNew subject after splitting |
|
Follow us on