1/9/2017 8:47 PM | |
Joined: 12/12/2008 Last visit: 5/20/2025 Posts: 69 Rating:
|
Hi, How is anybody(s) experience with stability with the IoT2000? A couple of questions: 1. Have you experienced a crash/hangup of the IoT2000? 2. In the case of answer "Yes" on point 1, do you know why, or for how long it did run? I only have one device, and it seems very stable to me. Just wondering if anyone had something to share on this point so anyone can know as much as possible about this point. /Ben ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/10/2017 11:57:38 AMNew subject after splitting |
|
1/10/2017 7:26 PM | |
Posts: 30 Rating:
|
The Intel Quark processor has a flaw where the lock prefix instruction will cause it to segfault. Because of this, everything for the image is compiled with -Wa,-momit-lock-prefix=yes. Everything you compile yourself should also be compiled with this AFAIK. This setting is located/shown in: https://github.com/siemens/meta-iot2000/blob/master/meta-iot2000-bsp/conf/machine/iot2000.conf |
This contribution was helpful to
1 thankful Users |
1/10/2017 8:43 PM | |
Joined: 2/10/2012 Last visit: 7/30/2025 Posts: 315 Rating:
|
Ah, thanks! The joy of open source! Now also at Siemens. No hiding but solving. If only pigs could fly.. |
1/13/2017 9:20 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by emit is split to a separate thread with the subject "Intel System Studio IoT Edition" and "IOT2000" connection has a problem. Best regards |
5/5/2017 2:37 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by sure94 is split to a separate thread with the subject Access IOT2040 without Putty. Best regards |
5/15/2017 1:28 PM | |
Posts: 69 Rating:
|
1. yes 2. Working with the opcua nodes. |
9/29/2017 12:11 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by c.rossati is split to a separate thread with the subject If install IOT in field what is the mantainance of capacity?. Best regards |
Follow us on