8/8/2014 12:36 PM | |
Posts: 2 Rating:
|
Hello I have problem using HSC on PLC 1214C DC/DC/DC. I need to use HCS to count pulses from 2 phase magneticsensor. I have enabled HSC1 and settings of HSC are in attached file. The problem is, when frequency of input signal is lower than 50Hz counter works fine but when freqency rises counter stops working(around 100Hz). But I need HCS to count up to 10Khz input frequency. I tried to measure input signal with oscyloscope andinput signallooks fine. Does anyone now what is causing this problem Thans for any help. David
|
Last edited by: CS Moderator at: 8/11/2014 1:24 PMnew subject after splitting from /tf/WW/en/Posts/89664#top |
|
3/6/2015 3:46 PM | |
Posts: 2 Rating:
|
Hi, I'm having problems with my settings. Where can i find your attached file, because i don't see anything. Kind regards, Mathijs |
10/4/2017 12:49 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by mojtaba.f is split to a separate thread with the subject Connection with 3 magnetic pickup to S7-1200. Best regards |
Follow us on