10/25/2017 3:52 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35920 Rating:
|
Here the programs for the master / master mode. The LOGO! 0BA7 unfortunately can send network outputs only to a slave, not to another master. In your program is now only 1 bit sent from one master to the other master, there is still with the solution I made with the block B075 (master 1, the server). If you want later to get more bits between the LOGO!s, then we have to go for another solution. Attachment0BA7_master_master.zip (330 Downloads) |
This contribution was helpful to
1 thankful Users |
10/26/2017 2:40 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by Gouda1234 is split to a separate thread with the subject Exchange several digital information between LOGO!. Best regards |
Follow us on